Hvordan kan vi hjælpe dig i dag?

What is the Maximum Requests of NOM as client per M580 CPU scan?

Question:
What is the Maximum Requests of NOM as client per M580 CPU scan?


Answer:
It is 32 maximum requests in terms of BMEH582040.
It is 80 maximum requests in terms of BMEH584040.
It is 96 maximum requests in terms of BMEH586040