Vores varemærker

Velkommen til Schneider Electrics website

Velkommen til vores website
		
Hvordan kan vi hjælpe dig i dag?
What are the considerations for PM3255 digital input and output ?

Issue

What are the considerations for PM3255 digital input and output?

Product Line

PowerLogic PM3000 Series (PM3255)

Environment

PM3255 Power Meter – Digital Inputs and Outputs

Resolution

  • The digital outputs of the PM3255 are polarity independent, meaning they do not require a specific polarity for proper operation.
  • The digital inputs and outputs of the PM3255 are electrically independent, so they function separately without electrical interaction between them.