Is the Schneider MBX Driver 8.1 compliant with Windows 10?
The Schneider MBX Driver 8.1 is not compliant with Windows 10 but it is possible changing registry keys to make it. Please follow procedure as describe inside the PDF file ; note that must be done before to install the Schneider MBX Driver 8.1.