How to link the DTM of multiple same type devices to a resuseable DFB
Issue
How to link multiple DTM's to a resuseable DFB
Product Line
Unity
Environment
Windows 10
Resolution
The following steps will demonstrate how to link multiple DTM devices of the same type to a common reuseable DFB.


Assign the DDDT type to the appropriate input/output of the DFB.
How to link multiple DTM's to a resuseable DFB
Product Line
Unity
Environment
Windows 10
Resolution
The following steps will demonstrate how to link multiple DTM devices of the same type to a common reuseable DFB.
- Create the DDDT types.
Assign the DDDT type to the appropriate input/output of the DFB.
Udgivet til: Schneider Electric Danmark