SCADAPack Workbench CAM5 - Bit to Word / Word to Bit Example
These SCADAPack Workbench CAM5 "Bit to Word" and "Word to Bit" function block examples provides a convenient method to access individual bits in a 16-bit value. The Bit2Word function block allows you to pack bit information into a 16-bit value.
These sample programs are intended to demonstrate one or more programming functions or methods and are presented as programming examples only. Schneider Electric assumes no liability for the use or application of these example programs or any portion thereof.
These sample programs are intended to demonstrate one or more programming functions or methods and are presented as programming examples only. Schneider Electric assumes no liability for the use or application of these example programs or any portion thereof.