Vores varemærker

Impact-Company-Logo-English Black-01-177x54

Velkommen til Schneider Electrics website

Velkommen til vores website
		
Hvordan kan vi hjælpe dig i dag?
Where can I find the Profinet GSD file for the ATV600 and ATV900 drives?
Issue:
Where can I find the GSDML file for ProfiNet to use with the Altivar 630 or Altivar 930 drives?

Product Line:
Altivar 630 and 930

Environment:
All serial numbers for Altivar 630 and 930

Cause:
GSD file for profinet

Resolution:
https://www.se.com/ww/en/download/document/PROFINET_GSDML_VW3A3627/