Hvordan kan vi hjælpe dig i dag?

Does the drive ATV930 have direct torque control?

Issue:
Availibility of Direct torque control on the ATV930

Product Line:
ATV930

Environment:
All serial numbers

Cause:
N/A

Resolution:
We do have torque control. There is an algorithm called Direct Torque Control. We don't use that exact algorithm, but it is very similar control.