Hvordan kan vi hjælpe dig i dag?

Is there an adjustment to reduce motor oscillation in the ATS48 softstart?

Issue:
Adjustment to reduce motor oscillation in the ATS48.

Product Line:
ATS48

Environment:
All

Cause:
Motor is making a imbalance noise during start and stop.

Resolution:
Stator loss compensation 0 to 90%     default  50%
Parameter active in acceleration phases (and deceleration phases if StY is set to -d-).
In the event of torque oscillations, reduce this parameter gradually until the device is functioning correctly.
Oscillations are most common if the soft starter is connected in motors with excessive slip.