Vores varemærker

Velkommen til Schneider Electrics website

Velkommen til vores website
		
Hvordan kan vi hjælpe dig i dag?
What is the ATV320 24Vdc power supply rating?

Article available in these languages: Spansk

Issue:
Planning external uses for the available 24Vdc power supply from the ATV320.

Product line:
ATV320, Altivar 320

Environment:
n/a

Cause:
n/a

Resolution:
The Altivar 320 power supply is rated for 100mA load.  Tolerance of the voltage supply is -15% to +20%.
Note that the logic inputs use 7mA each.