What are the main features of PM1130H meter ?
Issue:
Need a quick summary of the main capabilities/features supported by the PM1130H meter.
Product Line:
PM1130H meter
Environment:
Using the PM1130H as a stand-alone meter or as part of an energy management system
Local interaction via front panel / display
Communications via RS-485
Applications requiring energy monitoring, power quality, and basic cybersecurity controls
Cause:
Users often need a consolidated list of the PM1130H’s key features to confirm whether it meets monitoring, accounting, communications, power quality, and access-control requirements.
Resolution:
The PM1130H meter supports many features, including:
- LED display screen: Intuitive self-guided navigation using four buttons; LED display with three lines of concurrent values and a load bar indicating current loading.
- Energy accounting and balancing
- Relay (PM1130H only), alternate source, and RS-485
- THD% for voltage and current, per-phase
- Active, reactive, and apparent energy readings
- Cybersecurity: Ability to disable the RS‑485 port using front panel keys to help prevent unauthorized access; can also be used for toggling between RTU devices when software systems have limited node availability
- Measurement of True power factor (True PF)
You can use the meter as a stand-alone device, but its extensive capabilities are fully realized when used as part of an energy management system.