Hvordan kan vi hjælpe dig i dag?

Is the PowerLogic BCPM (Branch Circuit Power Meter) compatible with NQ and NF panels?

Issue
Is the PowerLogic BCPM (Branch Circuit Power Meter) compatible with NQ and NF panels?

Product Line
Power Logic Branch Circuit Power Meter (BCPM)

Environment
Mounting considerations and installation

Cause
Compatibility between older BCM and newer BCPM meters in NQ, NF and NQOD panels.

Resolution
As of April 2010 the BCPM is fully compatible with the NQ and NF panels.  The NF panels are designed for 1" spacing and the NQ panels are designed for 3/4" inch spacing. The older BCM (Branch Current Meter) is only compatible with the NQOD panels.