Hvordan kan vi hjælpe dig i dag?

Can we use Lexium 05 for BMH motors?

No. It is not possible to drive BMH from LXM05. The LXM05 needs a temperature sensor and the BMH has no sensor.
LXM05 cannot drive BMH. Only BRH, USH, BSH and SER can be driven by LXM05.