Hvordan kan vi hjælpe dig i dag?

How many BMXNOR0200 module we can have with Modicon M340 CPU

The maximum Ethernet port for M340 CPU system is 3 including the port on PLC. Therefore, a maximum of two BMXNOR0200 modules
can be inserted in a M340 system.