Hvordan kan vi hjælpe dig i dag?

How to enable Additional Debugging in ION setup when uploading a DCF file into an ION meter?

Issue
The Template LOG is required for advanced troubleshooting of issues occurring in an ION meter.

Product Line
PowerLogic PM8000 series meters
ION 7550 series meters
ION 7650 series meters
ION 8600 series meters
ION 8650 series meters

Environment
Troubleshooting

Resolution

  1. Navigate to setup assistant-->Template-->Send to meter
  2. Hold "SHIFT" and click on send. The following Window appears.


Additional debugging enabled

  1. The Template LOG is located in the following directory:

C:\ProgramData\Schneider Electric\ION Setup