Vores varemærker

Velkommen til Schneider Electrics website

Velkommen til vores website
		
Hvordan kan vi hjælpe dig i dag?
How to connect an ATV320 to a HMI to save the parameters of the drive
Question:
How to connect an ATV320 to a HMI to save the parameters of the drive

Product String Reference:
  1. Top Level > Product Category > Industry > Industry Control & Drives > Variable Speed Drives > Altivar 320.
  2. Top Level > PR_Product_OPS_Structure > Variable Speed Drives and Soft Starters > Low Voltage AC Machines Drives > Altivar Machine ATV320

Objective:
The objective of this video is to provide guidance of how to connect an ATV320 drive to HMI device.



Product Line:
IDSDS – Speed Drives Systems.

Environment:
N/A

Resolution:
  1. Connect the RJ45 adaptor to the ethernet cable running to the drive
  2. Connect the HMI to the RJ45 adaptor. The display of the drive will now be apparent
  3. To save the parameters of the drive, go to the Main Menu, and scroll to “Open / Save As”
  4. Select “Save As”
  5. Select “File” that is free. The file will now transfer from the Drive to the HMI.