Hvordan kan vi hjælpe dig i dag?

How to set up ATV630 for profibus communication?

Issue:
Setting up ATV630 for profibus communication.

Product Line:
Altivar 630

Environment:
All

Cause:
Setup

Resolution:
1) Set profibus address - [Communication] / [Comm Parameters] / [Profibus]
(PbC-)
2) Set reference frequency to communication module - [Complete settings] / [Command and Reference] / [Ref Freq 1 Config]

That is is all on drive side, all others has to be configured in the PLC.