Hvordan kan vi hjælpe dig i dag?

What is the resistance for the VZ3G1104 temperature probe?

Issue:
Wants to test the temperature sensor to make sure it is still working properly.

Product line:
Altivar 61/71, ATV61 ATV71

Environment:
n/a

Cause:
Overheating

Resolution:
The resistance of the temperature probe should be 5k ohms at 25C.