Vores varemærker

Velkommen til Schneider Electrics website

Velkommen til vores website
		
Hvordan kan vi hjælpe dig i dag?
What are the mounting options for Legacy 784 series relay sockets?
Issue:
Mounting options for Legacy 784 series relay sockets.

Product Line:
Legacy General Purpose Relays

Environment:
784 Series Accessories

Resolution:
Socket part number is 70-784D14-1. It is used for 784XDX relays. Socket is panel mounted. It can be mounted on a DIN rail using an adapter with part# 16-784C. It can also be Flange mounted using part number 16784C1 adapter.