Hvordan kan vi hjælpe dig i dag?

How to run Modsoft in Windows 10.

Issue
How to run Modsoft in Windows 10.

Product Line
Modsoft

Environment
Windows 10

Resolution
Modsoft is considered to be obsolete.  There is no longer any Engineering support for the product.  It is recommended to update to either 'ProWORX 32'
or 'Control Expert'.

Modsoft is a DOS based program.  In order to run Modsoft in Windows 10, the PC will need to have either

  • A DOS emulator
  • NTVDM.dll installed.
  • Windows XP running in a virtual machine.


The following articles can be referenced on running a DOS based program in Windows 10.

https://www.howtogeek.com/228689/how-to-make-old-programs-work-on-windows-10/