Hvordan kan vi hjælpe dig i dag?

How do you program an ATV320 to stop with a freewheel stop rather than ramp stop?

Issue:
Programming ATV320 to coast to stop rather than a controlled stop

Resolution:
ATV320 default stop is ramp stop. When you need the motor to coast to stop instead of ramp stop, adjust parameters as follows.  Navigate on the display to ConF > FULL > Fun > Stt- > Stt.  The factory setting is rMP, change this to nSt.

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:

Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)