Vores varemærker

Velkommen til Schneider Electrics website

Velkommen til vores website
		
Hvordan kan vi hjælpe dig i dag?
How to set the output frequency to show on the ATV320 display every time drive is powered on?

Article available in these languages: Czech

Issue:
Change the default display for when the drive is powered on to show output frequency.

Product Line:
Altivar Machines, Altivar 320

Environment:
All models and serial numbers

Cause:
Default display is Reference Frequency

Resolution:
Go to Non (1.2 Monitoring) menu, select rFr (output frequency), and press and hold ENT for more than 2 seconds.  Display will flash to indicate the change had been made.
To dispaly amperage: Go to NON > select NNO > LCr, ENT for more than 2 seconds