Hvordan kan vi hjælpe dig i dag?

Different licenses of Ecostruxure Control Expert are actives on the same PC but Ecostruxure Control Expert always starts the same license.

When Ecostruxure Control Expert starts working with a license (e.g. L), Ecostruxure Control Expert will always offer the features of this license, unless the user does a specific action. In case of multiple licenses and to select the one to use, it is mandatory first to close all Ecostruxure Control Expert application and to launch the PackageSelector.exe file.

The PackageSelector.exe file is on:
C:\Program Files (x86)\Schneider Electric\Control Expert 14.0\
Start PackageSelector with administrator right, click right on PackageSelector icon and select RUN as Administrator.
A screen is displayed and then it is possible to select the Ecostruxure Control Expert license that will be use next time that Ecostruxure Control Expert will start.

NOTA: Safety is an Add On, it is not part of the presented packages and so will be available.