Hvordan kan vi hjælpe dig i dag?

What is the part number of the replacement connector kit for ATV340 drive?

Issue :
Replacement connectors for ATV340 drive.

Product Line :
Altivar Drive

Environment :
ATV340, Altivar Machine, Altivar 340

Cause :
Lost connector kit

Resolution :
There are three different part numbers for the kit, depending on the drive frame size.  A single connector piece is not available, order the complete kit only.

connector part photo 1

Drive Frame Size 1
Part# VW3A34001
ATV340U07N4 ATV340U15N4 ATV340U22N4 ATV340U30N4 ATV340U40N4

Drive Frame Size 2
Part# VW3A34002
ATV340U55N4 ATV340U75N4

Drive Frame Size 3
Part# VW3A34003
ATV340D11N4 ATV340D15N4 ATV340D18N4 ATV340D22N4