What is Form Y190 for the 8940 Pump Panels?
Issue:
8940 modifications
Product Line:
Class 8940, Well-Guard Control™ Pump Panels
Environment:
Full Voltage, Type SS, XS
Resolution:
Form Y190 is only available on the Class 8940 Pump panels. This is to remove the existing Type S contactor and replace with 8502W vacuum contactors.
8940 modifications
Product Line:
Class 8940, Well-Guard Control™ Pump Panels
Environment:
Full Voltage, Type SS, XS
Resolution:
Form Y190 is only available on the Class 8940 Pump panels. This is to remove the existing Type S contactor and replace with 8502W vacuum contactors.
Udgivet til: Schneider Electric Danmark