Hvordan kan vi hjælpe dig i dag?

ION9000 and RFC standards or IPv6

Issue
Want to know if ION9000 supports the latest RCF standards 8200, 4443, 4861, 6724

Product
ION9000

Resolution
Following details are for ION9000 firmware version V2.1 and older

RFC 8200: Internet Protocol, Version 6 (IPv6) Specification
RFC 4443: Internet Control Message Protocol (ICMPv6) for the Internet Protocol Version6 (IPv6)
RFC 4861: Neighbor Discovery for IP Version 6 (IPv6)
RFC 6724: Default Address Selection for Internet Protocol Version 6 (IPv6)

V2.1 and older
RFC 8200No1
RFC 4443Yes
RFC 4861Yes
RFC 6724No2


1. ION9000 has support for previous version RFC 2460: Internet Protocol, Version 6 (IPv6) Specification
2. ION9000 has support for previous version RFC 3484: Default Address Selection for Internet Protocol version 6 (IPv6)