Function Implicit Type Conversion
Issue
User can be found an issue working with type to type operation at Control Expert.
Environment
Control Expert
Resolution
As per default the function Enable Implicit Type Conversion is not checked when the user create a new project. Then this function must be checked to avoid errors with the application. To activate this function:
1- Go to Tools > Project Settings > Program > Languages > Common
2- Enable implicit type conversion
For further details, see the document attached.