Hvordan kan vi hjælpe dig i dag?

How to locate an EGX150 physically?

Issue
A customer has accessed the web page of the EGX150 (aka, LINK150) and she is trying to locate the device easily among other devices in the installation site.

Environment
EGX150 or LINK150

Cause
The installation site is large and there are multiple EGX150 on site. The customer is trying to find an easy way to locate the EGX150 physically, provided she has access to the device's web page.

Resolution

To locate the Link150-XXYYZZ, select the Configuration & Settings menu, go to Device Location/Name submenu, click Device physical location, and then click Blink ON.

The RS485 LED of the selected Link150-XXYYZZ blinks for 15 seconds with 1 s ON and 1 s OFF (test mode).