Issue:
Why when using the Print function on Ecostruxure Machine Expert Basic v1.2 do I get a blank page in the POU section?
Product Line:
Ecostruxure Machine Expert - Basic v1.2
Cause:
Unfortunately, there is a known anomaly in the software causing this issue, there is a new Service Pack available to fix this.
Resolution:
From v1.2 SP1 this software anomaly was mitigated, therefore, you should update to the said version or above.
Link to download the newest version: https://www.se.com/us/en/download/document/MachineExpertBasic_V1_2_SP1_P1/
Note: Unfortunately, you cannot downgrade a project to open it with an older version of EME-Basic. For instance, you cannot open an EME-Basic v1.2 project with EME-Basic v1.1
Udgivet til: Schneider Electric Danmark