ZBRT2 does not send signal when slowly released.
The information we give for the ZBRT transmitters, the minimum actuation speed is 0,1m/s and the maximum force is 10N.
Actually, if the operator actuate very slowly the transmitter, it can affect the frames transmitted.
Udgivet til: Schneider Electric Danmark