How many batteries can I attach to the Smart-UPS Industrial XU2K0LLXXRCC & XU1K3LLXXRCC?
Issue:
How many batteries can I attach to the Smart-UPS Industrial XU2K0LLXXRCC & XU1K3LLXXRCC?
Product Line:
Smart-UPS Industrial XU2K0LLXXRCC & XU1K3LLXXRCC
Environment:
All serial numbers
Resolution:
The Smart-UPS Industrial UPS has a maximum capacity of 200Ah and uses a 12V 50Ah or 12V 100Ah lead acid battery.
APC offers the XB050XX1XS (12V 50Ah) or the XB102XX1XS (12v 100Ah). Battery harnesses XHXXS7A4F (4ft) and XHXXS7A8F (12ft) are also used.
To have the maximum capacity reached, you will need:
16 pcs of the XB050XX1XS (12V 50Ah) + 4 wiring harness
or
8 pcs of the XB102XX1XS + 2 wiring harness
For information on how to daisy chain the batteries/harness, please refer to the installation guide below:
Should you need further assistance, don't hesitate to get in touch with our Customer Care Center at https://www.apc.com/us/en/support/