Hvordan kan vi hjælpe dig i dag?

Replace a HMIG3U, can I use the system sd card from the failed unit in the new unit?

Issue:
If a HMIG3U unit fails, can I pull the System SD Card from the failed unit and insert it into the replacement unit and will power-up?

Product Line:
HMIG3U

Resolution:
Yes, if a HMIG3U unit fails.  You can pull the System SD Card from the failed unit and insert it into the replacement unit with the same model number.  The unit will power-up and boot to the application.

Schneider Electric Danmark

Se mere
Produkt:
Område:
Se mere
Produkt: