Hvordan kan vi hjælpe dig i dag?

Save the communication and operation report of an explicit communication like Read_Var EF using an ST section

In the Control Expert documentation, you can see the below :

Manage Parameters Communication and Operations Reports

See below an example of an ST section that will record the communication and operation report value of an explicit communication EF (So the Management_Table[1] of this EF) and will check and reset accordingly the function management parameters :

ST programming

This ST section is also available in attachment

Schneider Electric Danmark

Bilag
( Read_Var ETH ).txt [888 Bytes]
St section.zip [974 Bytes]