Hvordan kan vi hjælpe dig i dag?

Machine Expert String Length Longer Than 255

Issue:

In Machine Expert, i need a string length longer than 255

Resolution:

STRING

With EcoStruxure Machine Expert V2.2 and later versions, the STRING data type

can be encoded in Latin 1 or in UTF-8 format. For project-wide interpretation as

UTF-8, enable the parameter UTF8 Encoding for STRING in the Project

Settings > Compile options dialog box. For further information, refer to ProjectWide UTF-8 Encoding, page 580.

NOTE: Before you set the encoding format to UTF-8, execute the static

analysis rule SA0175 (refer to the EcoStruxure Machine Expert Menu

Commands Online Help for details) on your code to help detect constructs that

may cause issues with UTF-8 encoding.

NOTE: If you use UTF-8 encoding, add the {attribute 'monitoring_

encoding' := 'UTF-8'} pragma, page 554 to the declaration of a variable.

It allows you to monitor the contents of the variable in UTF-8 encoding.

A STRING data type variable can contain any string of characters. The size entry

in the declaration determines the memory space to be reserved for the variable. It

refers to the number of bytes in the string and can be placed in parentheses or

square brackets. If no size specification is given, the default size of 80 bytes will

be used. If a variable is initialized with a string too long for the variable data type,

the string will be correspondingly cut from right to left.

String length:

• For Latin 1 encoding, the memory space needed for a variable of type

STRING is 1 byte per character + 1 additional byte. This means, the

“STRING[80]” declaration needs 81 bytes.

• With UTF-8 encoding, one character can have a length of up to four bytes.

The length of the string indicates the number of bytes which are reserved for

the STRING. Thus, there is no longer a 1:1 relationship between the

character count and the string length in bytes.

Example of a string declaration with 35 bytes:

str:STRING(35):='This is a String';

In general, the length of a string is not limited. When you execute string

manipulations with the functions of the Standard library, strings up to a length of

255 are allowed. When you execute string manipulations with the functions of the

StringUtils library, longer strings (>255 characters) are also permitted.

When a variable of the data type STRING is reinitialized by resetting the

application, the contents of the old string, that exist after the terminating null

character of the initial value, are not overwritten. This applies both to initialization

with the initialization value and to initialization with the default initialization value of

0.

For further information, refer to WSTRING and STRING Constants (Operands),

page 686.

https://download.schneider-electric.com/files?p_Doc_Ref=EIO0000004321&p_enDocType=User+guide

NOTE: You can use implicit checks to validate the conversion of variable

types (refer to the chapter POUs for Implicit Checks, page 175).

NB.

See more on Page 662 of 1220

https://download.schneider-electric.com/files?p_Doc_Ref=EIO0000004321&p_enDocType=User+guide

Project settings compile options UTF8