Hvordan kan vi hjælpe dig i dag?

BMENUA0100 Login Advanced eller Secured og Standard mode

Standard login til BMENUA0100 er følgende:

Default IP: 10.10.MAC5.MAC6

The default username / password combination depends on the cybersecurity operating mode setting:

• Advanced (or Secured) mode: SecurityAdmin / AAAAAAAA

• Standard mode: installer / Inst@ller1

NOTE: You will be asked to modify the password upon first use in Advanced (or Secured) mode. Verify your local laws and regulations whether this is a requirement.

Se evt. side 32 her: Link

Schneider Electric Danmark

Se mere
Produkt:
Se mere
Produkt: