Electrical safety solutions for commercial and industrial installations
Protect people, assets, and operations from electric shock, arc flash, electrical fire, fault current, and equipment damage through safer design, protection, monitoring, and maintenance.
Electrical safety solutions for commercial and industrial installations
Electrical safety combines practices, standards, and technologies that prevent arc flash, electric shock, electrical fire, and equipment failure. Effective design and risk assessment reduce injuries, asset damage, and operational downtime.

Protect people
Reduce exposure through grounding, bonding, protective devices, safer design, and safe work practices.
Protect assets
Limit thermal and mechanical stress through correctly rated equipment, faster interruption, monitoring, and maintenance.
Maintain safety over time
Detect abnormal conditions such as overheating or insulation degradation, through monitoring and regular testing.
Electrical safety priorities vary by installation. Industrial facilities and commercial buildings require different approaches to protection, continuity, and maintenance.

Industrial facilities
Protect people and critical operations in demanding electrical environments. Address high fault currents and arc flash risks across medium-voltage, motor-control, and critical production systems with coordinated protection, fast fault clearing, and condition monitoring.Electrical safety is achieved by designing installations to IEC standards. Explore the main topics.

Prevent electrical fire
Reduce risks related to overheating, loose connections, insulation failure, and electrical faults.Talk to an electrical safety expert

Assess
Conduct an electrical and arc-flash risk assessment.
De-energize
De-energize whenever possible and verify zero energy.
Engineer
Apply grounding, bonding, and protection coordination.
Select
Choose devices with suitable voltage, current and breaking-capacity ratings, per IEC.
Clear fast
Reduce fault-clearing time and incident energy.
Monitor
Detect abnormal heat and equipment conditions early.
Maintain
Inspect, test, and maintain the installation regularly.
Work safely
Use appropriate work practices and PPE.
Learn how these two topics are addressed in the design and operation of electrical installations.

Electrical fire prevention in electrical systems
Prevent fires caused by faults, overheating, and insulation failure through appropriate system design, protection devices, and compliance with IEC 60364.
Low-voltage protection and arc flash mitigation
Protect people and property from overload, short-circuit, earth-fault and arc-related risks with protection devices and well-designed systems.Discover solutions that help protect people, equipment, and electrical installations.
Electrical safety risks include electric shock, arc flash, electrical fires, equipment overheating, short circuits, and other electrical faults. Risk can be reduced through appropriate system design, grounding and bonding, protective devices, monitoring, maintenance, and safe work practices.
Electrical fire prevention starts with appropriate electrical system design and protection. Correctly rated protective devices, arc-fault and residual-current protection where applicable, connection and temperature monitoring, regular inspection, and preventive maintenance can help identify and limit conditions that may lead to electrical fires.
Electrical grounding, or earthing, provides a defined path for fault current and helps protective devices operate when an electrical fault occurs. Correct grounding and bonding can reduce dangerous touch voltages and are fundamental parts of electrical shock and fault protection.
Fault-current protection detects abnormal electrical conditions and isolates the affected part of an installation. Correct device selection and protection coordination can help reduce fault duration, limit equipment damage, and avoid unnecessary interruption of unaffected parts of the electrical system.
Continuous condition and temperature monitoring can help identify abnormal heating in cables, connections, and electrical equipment before visible damage or failure occurs. Combined with inspection and preventive maintenance, early detection can help reduce the risk of equipment damage and electrical fire.
An arc flash is a sudden release of electrical energy through an unintended electrical arc. Risk-reduction measures can include de-energising equipment whenever possible, reducing fault-clearing time, appropriate system design and protection, remote operation, safe working distances, and arc-rated PPE based on an arc-flash risk assessment.
Applicable requirements depend on the installation, activity, and country. Relevant references can include IEC 60364 for low-voltage electrical installations, NFPA 70E for electrical safety in the workplace, and IEEE 1584 for arc-flash incident-energy calculations, together with applicable national regulations and requirements.
Choose a topic: electrical worker safety • fire prevention • system design • product selection
Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales enquiry online and an expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Center
Find support resources for all your needs, in one place.