Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Which contactors are used in the LG and LJ TeSys enclosed starters?

The contactor used will be indicated by the part number itself as shown in examples below:

Regarding the type:

  • LG7K******- denotes that the contactor is a TeSys K contactor
  • LG7D****** - denotes that the contactor is a Tesys Deca contactor

Regarding the size:

  • LG7K06**** - denotes that the contactor will be a 6A Tesys K (LC1K0610**) (Tesys K contactors are always the versions with N/O auxiliary)
  • LG7D09**** - denotes that the contactor will be a 9A Tesys Deca (LC1D09**)

Regarding the coil voltage:

  • LG7K06B7** - denotes that the contactor will be a 6A Tesys K with 24V AC coil (LC1K0610B7)
  • LG7D09B7** - denotes that the contactor will be a 9A Tesys Deca with 24V AC coil (LC1D09B7)

The final 2 characters of the part code relate to which motor circuit breaker is included in the starter:

  • LG7K06B706 - denotes that the circuit breaker is GV2ME06, rated 1...1.6A
  • LG7D09B714 - denotes that the circuit breaker is GV2ME14, rated 6...10A

Schneider Electric Ireland
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
  • Help and Contact Centre