Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What earthing devices are available for use with SAIF fuseways?
Earthing devices are available for busbar or circuit earthing on SAIF fuseways are:
Type ED6, for 630A & 800A fuseways.
Type ED4, for 400A fuseways.

Pillars manufactured for MOD sites, i.e. to DEO Works specification 039, require special earthing devices.

Schneider Electric Ireland

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre