Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the differences between GV3ME and GV3P Motor Protection Circuit Breakers (MPCB)?

The differences between GV3ME and GV3P are as follows:

Operation

GV3ME* was a pushbutton operated device whilst GV3P is rotary knob operated.

The rotary knob has a number of advantages:

  • Switch position/state is more easily visible.
  • The rotary knob has a trip position as well as an "Off" position making it easy to detect if the device has tripped or been switched off.
  • The rotary knob can be fitted with an external handle and shaft with door interlock.

Power connections

GV3P uses the Everlink cable clamp system which means:

When correctly tightened in the first instance, the cable clamps will not need re-tightening. The design of these removable clamp systems also means that Everlink devices can be coupled together without connecting adaptors

Electrical values
GV3ME current ranges began at 1 to 1.6A in the GV3ME06
GV3P current ranges do not start until 9-13A in the GV3P13

The difference between the two is covered by the GV2ME and GV2P ranges, each ranging from 0.1 to 0.16A to 24 to 32A. Again, the difference between GV2ME and GV2P is in the operation, with ME being pushbutton controlled and P being rotary knob controlled.

In some values the GV3P has greater breaking capacity.

Dimensions
The GV3P is narrower on the DIN rail, the GV3ME being 61.2 w x 120 h footprint and 113mm deep.
The GV3P is  55 w x 132 h footprint and 136mm deep (all dims in mm)

Accessories
GV3P use the same auxiliary contacts and accessories as the GV2 range whereas the GV3ME had their own range of devices.

Schneider Electric Ireland

Attachment(s)
GV3P and Accs refs and accs.pdf [319.09 KB]
GV3 ME Series.pdf [2.77 MB]
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
  • Help and Contact Centre