The new enclosures GV3PC aren’t suitable for GV3ME because of the handle.
But there is an enclosure that can take the new GV3P and GV3L, plus there is space to mount a contactor inside.
But there is an enclosure that can take the new GV3P and GV3L, plus there is space to mount a contactor inside.
This enclosure is available with 2 different handles, see below details
Enclosed thermal-magnetic MCB GV3 (TeSys enclosed starters – for customer assembly)Note: GV3PC01 and GV3PC02 existed previously but with different characteristics, these new enclosures replaced the old with same part number.
The older enclosures only had room for the GV3, had lower IP rating, IP55, different dimensions and the handle was different.
Released for:Schneider Electric Ireland