Yes it is possible to use single phase MCB's in the three phase distribution board, however, this is not good practice for the following reasons: 
 
- Damage to Motors - Motor loads or circuits that are critical to have three phase voltage may be damaged by the loss of one phase. This is often called "Single Phasing".
 - Danger to personnel - Someone working on the installation may assume that the fault on a three phase load has disconnected all three phases, but two are still connected
 - Danger to equipment - The fault was caused by a problem with the installation, therefore it would be good to disconnect the load from the three phase device
 
Released for: Schneider Electric Ireland