{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the radius of curvature of an ASI cable?
The TPE ASi cable, XZCBxxxxxH, has been tested for flexible mounting: 300,000 operations.

It is preferable to use the TPE version, part number XZCBxxxH, as the radius of curvature behavior with regard to the thickness is better than the standard cable.

For the standard cable, the radius of curvature of the XZCB flat rubber cable is:
  • 15 mm across the thinnest section
  • 0 mm across the thickest section.

The radius of curvature of the XZCB TPE cable is:
  • 20 mm across the thinnest section
  • 60 mm across the thickest section.
ASI

Schneider Electric Ireland