Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is Modbus serial / TCP (ethernet) communication possible with the Zelio logic modules?

Both Modbus Serial and Ethernet communication are possible but only with Zelio logic SR3 modules supplied with 24 VDC (SR3B... BD).

The SR3MBU01BD communication extension must be used for serial, or SR3NET01BD for Ethernet Modbus / TCP.

Modbus Module for Zelio SR3


For more information on using this module, refer to the Zelio SR2/SR3 catalogue. You can find this, along with other relevant documentation, on our website www.se.com/uk/



Just type your part number into the search bar and click on the result.

Schneider Electric Ireland

Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre