{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the minimm value of the current rating that can be set on the MGP style moulded case circuit breakers?
MGP style MCCB can be fitted with TMD trip unit, or Micrologic trip unit.

Below are the minimum current rating for each:
TMD trip units up to 250Amps, can be set from 70% to 100% of the nominal value.
e.g. for a 250A TMD unit from 175A to 250A

Micrologic 2 trip unit on 40, 100, 160, 250, 400& 630A, can be set from 40% to 100% of the nominal value.
e.g. for a 400A Micrologic 2 unit the valuse are from 160A to 400A

Schneider Electric Ireland