What can the MGP0803X & PP40803X be turned down to?
MGP & PP4 style breakers with the thermal magnetic(TM***D) trip can be turned down to 70% of their nominal value, In the case of the MGP0803x then the adjustment is: 80A x 0.7 = 56A
Released for:Schneider Electric Ireland
Explore more
Range:
ComPact NSX
Powerpact 4
Articles that might be helpful
Show more articles
Discuss this topic with experts
Visit our Community for first-hand insights from experts and peers on this topic and more.