Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to define the part number of NSX Vigi unit for earth leakage detection?


To define the part number of the vigi unit, you need to identify the frame size (current rating) and number of poles of the NSX breaker to be attached to the vigi module.
Use the attached PDF file and selection chart to help you determine the correct Vigi Unit for the intended application.
i) For Type and Sensitivity see the NSX catalogue 2022, pages B22-B25
ii) For Product part number see selection chart below.

A four pole vigi unit can be installed on a three pole MCCB  if the following part number LV429214 is used. There are also other factors to take into account if the distribution board has a neutral then you would need to also fit a neutral linking kit to the vigi unit part number NSNL250 for up to 250A and part number NSNL630 for up to 630A.

Vigipact Part References

Vigi module selection chart

Schneider Electric Ireland

Attachment(s)
Comapct NSX.pdf [84.64 MB]
Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:

Need help?

  • Product Selector

    Quickly and easily find the right products and accessories for your applications.

  • Where to buy?

    Easily find the nearest Schneider Electric distributor in your location.

  • Help Centre

    Search topic-related frequently asked questions to find answers you need.

  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre