{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What information is contained in the cartridge of the Sepam series 80?
The cartridge of the Sepam series 80 contains the following information:
- system and application software (protection functions, settings and parameters)
- customised command and control functions (matrix, equation editor, customised logic, etc.)
- customised operating language.
This information is saved if a power failure occurs on the Sepam.
Caution: never remove the cartridge when the Sepam is powered up.

Schneider Electric Ireland