Search FAQs
Osisense XCC - Reliability data of the XCC1514TR11RNL5 encoder like MTTFD
The reliability data of the XCC1514TR11RNL5 encoder,are the following :
- MTTF = 70.5 years (mean time to failure),
- MTTFD = 141 years (mean time to dangerous failure),
- DC = 0 (diagnostic coverage) of the sensor alone,
- mission time = 20 years.
They are used for the functional safety, according to the ISO 13849-1 standard (Performance Level). The products are not safety components according to the machine directive 2006/42/EC
- MTTF = 70.5 years (mean time to failure),
- MTTFD = 141 years (mean time to dangerous failure),
- DC = 0 (diagnostic coverage) of the sensor alone,
- mission time = 20 years.
They are used for the functional safety, according to the ISO 13849-1 standard (Performance Level). The products are not safety components according to the machine directive 2006/42/EC
Released for:Schneider Electric Ireland
Explore more
Explore more