Search FAQs
Safety light curtains XU - Manufacture date of the XUSL4E or XUSL2E light curtains
The manufacture date of the XUSL4E or XUSL2E light curtains is a part of the serial number. The serial number is composed of the manufacture date and a progression number. Example in the attached picture showing the XUSL4E3BB081N transmitter and receiver serial number indicated on the labels : 14030740 where 14 is the production year (Y=2014), 03 is the week of the year (W=03) and 0740 is a progression number
Released for:Schneider Electric Ireland
Attachment(s)
Explore more
Explore more