Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How do you change the M221 so that it runs as soon as it is powered ?

By default the software configure the controller to be "Start in Previous State", however this value can be changed:

Image1
There are four possible states for the Starting Mode parameter:

  • Start In Previous State : The logic controller starts in the state that it was in before it was stopped
  • Start in Stop : The logic controller does not automatically start application execution
  • Start in Run : The logic controller automatically starts application execution given run criteria, such as the presence and charge of a battery, are met.
  • Unconditional start in Run : The logic controller automatically starts application execution even if the controller battery is absent or discharged.


The video below shows how the SoMachine basic (Now known as EcoStruxure Machine Expert Basic ) program is configured and loaded in to the M221 Controller

Schneider Electric Ireland

Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more

Need help?

  • Product Selector

    Quickly and easily find the right products and accessories for your applications.

  • Where to buy?

    Easily find the nearest Schneider Electric distributor in your location.

  • Help Centre

    Search topic-related frequently asked questions to find answers you need.

  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre