Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the short circuit rating of the Isobar P Distribution Boards?
The single phase Isobar Distribution Board has a fully type tested conditional short circuit rating of 16kA to BS EN 61439-3

The three phase Isobar Distribution Board has a fully type tested conditional short circuit rating of 25kA to BS EN 61439-3 when fed by an MCCB.

This applies to both the older Acti9 Isobar and Isobar P Style of boards.

Schneider Electric Ireland
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
  • Help and Contact Centre